Post Go back to editing

Remote Control of Evaluation Boards for ADMV1013/14

Category: Software
Product Number: ADMV1013

For my testing setup and evaluation purposes I needed to remotely control the eval boards for the ADMV1013/14. As discussed in this thread it is not possible to do this from a Linux workstation without elaborate workarounds. In the end I had to modify the hardware which does not feel too good on a 2000€+ board.

So it would be really great if one or more of those or similar suggestions could be implemented in the future (and is already available for other board):

- The board can be controlled via iio

- The source code for the PIC controller is available to be easily adapted

- The communication protocol for the dev board is be documented

- There is a connector (and some jumpers) for external SPI

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.