Post Go back to editing

SC1894_input signal bandwith

Thread Summary

The user inquires about the SC1894's ability to linearize at 12.5KHz and 25KHz input signal bandwidths with a target cancellation of 30dBc. The final answer suggests using the SC1894 00N13 version for narrowband signals, noting that 30dBc IMD correction is possible but depends on the power amplifier's characteristics. The user provided additional details: RF input frequency range 156.0125-162.0375MHz, input power level 0dBm, modulation schemes QPSK, 8PSK, 16QAM, 64QAM, and CDMA, peak-to-average ratio 3-6dB, and PA output power 12W (LDMOS 60W).
AI Generated Content
Category: Datasheet/Specs
Product Number: SC1894

Dear team,

Input signal bandwith of developing system is 12.5KHz and 25kHz.

Can SC1894 linearize at this input signal bandwidth?

Target cancellation is 30dBC

I am looking forward to your support.

Thank you.

Best & Regards,

Josh

  • Hello,

    Please help to share below details.

    1. RF Input frequency range to SC1894
    2. Input channel width- 12.5 and 25KHz
    3. Input power level(dBm) to SC1894
    4. Modulation scheme (QPSK/QAM/ other) of signal
    5. Peak to average ration of signal
    6. Power amplifier output power, P1 dBm, P3dBm
    7. Type of power amplifier and process
    8. PA output ACLR (dBc) without correction
    9. Expected ACLR correction 30 dBc
    10. Any up converter or down converter planned to use?
    11.  If yes pls share frequency details.

    Thank You

    RF products support team.

  • Dear team,

    refer to the following comments.

    1. RF Input frequency range to SC1894
       ==>156.0125~162.0375MHz
    2. Input channel width- 12.5KHz and 25KHz
      ==>Input channel bandwidth is 12.5KHz, 25KHz
    3. Input power level(dBm) to SC1894
      ==> About 0dBm(adjustable)
    4. Modulation scheme (QPSK/QAM/ other) of signal
      ==>QPSK&8PSK&16QAM&64QAM&CDMA etc
    5. Peak to average ration of signal
      ==>3~6dB
    6. Power amplifier output power, P1 dBm, P3dBm
      ==> Average outpower : 12Watt (LDMOS Tr : 60Watt)

    7. Type of power amplifier and process
      ==> LDMOS
    8. PA output ACLR (dBc) without correction
      ==> about 30 dBc
    9. Expected ACLR correction 30 dBc
     ==>Need to 30 dB improvement
    10. Any up converter or down converter planned to use?
     ==> No
    11. If yes pls share frequency details.

    Thank you.

    Regards,

    Josh

  • Hello,

    There are a couple of versions of the SC1894.  The 00C13 version and the 00N13 version.  The C13 version is for typical 4G/5G wireless cellular infrastructure applications though it can be also used with other signals.  The N13 version is for narrowband signals such as are used in public safety or satellite communication applications.  The only difference is in the firmware.  The C13 version will not work with such narrowband signals, so the N13 version is the only option.  Read the FW4.5.01.00 Release Notes doc downloadable from the SC1894 product web page to learn more about the narrowband part.

    Based on the given specs, I think there is a possibility the N13 part may be usable.  With narrowband signals, it is the Intermodulation Distortion (IMD) products that are of primary concern.  If one has two more more narrowband carriers, there will be many IMD products generated due to the non-linearity of the power amplifier (PA).  The SC1894 will attenuate these IMDs, but the amount of attenuation is highly dependent on the PA.  30dB or so IMD correction has been observed but it will depend on your particular PA.  Another factor is that if the PA is driven so hard that it is clipping the peaks of the signal, there is critical information on the PA non-linearity, which the SC1894 requires for linearization, that is lost.  This is sometimes the case in satellite communications.  If there is just a single carrier, the distortion immediately adjacent to the carrier will have little or no attenuation, especially with a 12.5KHz carrier.  If the ACLR requirement is referring to this adjacent distortion, then I think there is no way to support this.

    Regards

    Andrew

  • Hi Addrew,

    Thank you for your support.

    Regards,

    Josh

  • Hi AndrewBG,
    on your opinion, what should be the best ADI solution (if exists) to linearize a PA that works with HF (1MHz to 30MHz) range with minimum signal BW of 3KHz (for non AM signal). The possible signal's modulation can be AM or FM, or digital like QAM.
    I think that there's no solution for DPD, maybe a static analog predistortion, using MAX2009 or MAX2010 (with down/up conversion) , can works....
    Regards
    Giuseppe

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.