Post Go back to editing

how do I know LD clock frequency?

Category: Datasheet/Specs
Product Number: HMC833

Hi,

I'm using the HMC833 for obtaining a 2.2GHz carrier with a 38MHz in fractional mode. I have some issues with the lock stability and from previous experiences with the part I know they are normally solved by tuning the values in Reg07h:

  • Reg07h[2:0] lkd_wincnt_max
  • Reg7h[9:7] LD Digital Window duration

In order to choose reasonable values for them, I'm trying to understand better the theory of operation described in the data sheet, in particular the following paragraph:

Setting Reg 07h[6]=1 will result in a variable length lock detect window based upon an internal digital timer. The timer period is set by the number of cycles of the internal LD clock as programmed by Reg 07h[9:7]. The LD clock frequency is adjustable by Reg 07h[11:10]. The LD clock signal can be viewed via the GPO test pins. Refer 1.16 for details.

 , but the information in tha data sheet on Reg 07h[11:10] says 00=fastest, 11=slowest...Ok, but how fast or slow? How can I derive the LD clock frequency in order to figure out the duration of the lock window I want to set?

Thanks advance

Rodrigo

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.