Post Go back to editing

Questions about LT5546 operation

Category: Hardware
Product Number: LT5546

Hello
I have two questions about the LT5546.

Question 1
Is it possible for the LT5546 to output IOUT and QOUT in reverse after startup?

Question 2
I want to reduce the current consumption by switching between Shutdown Mode/Standby Mode/Normal Operation Mode, but
when I control it from Normal Operation Mode to Shutdown Mode to Normal Operation Mode, the QOUT signal seems to be incorrect.
On the other hand, the IOUT signal seems to have the correct value.

I can obtain the desired value by continuing in Normal Operation Mode.

Are there any restrictions when using "Shutdown Mode/Standby Mode/Normal Operation Mode"?
It is not expected that the operation mode will be switched in 5 ms cycles, etc.

I would appreciate any advice on concerns.

For reference, I have attached the waveform of the QOUT+ signal when monitored.

I would appreciate your reply.

Best Regards,
Knj