May i know what is the Failure rate (FIT) for HMC986A and is it prone to hydrogen poisoning?
Thank you!
KCC's Quizzes AQQ306 about a fish stick challenge
1. First the quote of the month: " I am so clever that sometimes I don't understand a single word of what I am saying" - Oscar Wilde
2. New quiz AQQ306 about a fish stick challenge:
Here below is a pseudo fish diagram swimming to the right.
Question
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
HMC986A
Recommended for New Designs
The HMC986A is a reflective, single-pole, double throw (SPDT) switch, manufactured using a gallium arsenide (GaAs) process. This switch typically provides...
Datasheet
HMC986A on Analog.com
May i know what is the Failure rate (FIT) for HMC986A and is it prone to hydrogen poisoning?
Thank you!
Hi,
HMC986A is sensitive to hydrogen poisoning.
The 90% MTTF is 1.52x10^10 hours at 85C.
Okay thanks for the information!
Do you have the HTOL data for this?
On top of that, do you also have the data in 60% fit rate at 85degC?
60% MTTF is 3.82x10^10 hours at 85C.
As for the HTOL data, the effort involves lots of generics sharing the same process, yielding with the total equivalent device hour to come up with FIT calculations. Considering the acceleration factor and number of samples, the equivalent total device hours is 3.49x10^10. The failure rate was calculated using Chi Square Statistic.
oh alright. To confirm the fit rate is 3.82x10^10 not 3.82x10^-10 right?
Sorry about the confusion, these are MTTF values ( 10^9 / FIT )
MTTF (90%) = 1.52 x 10^10 hours
MTTF (60%) = 3.82 x 10^10 hours
Since you know the Failure rate, do you know what is the activation energy to calculate it?