Hi
I would like to use this mixer as Upconverter from 1.3GHz to 11.5GHz
Can I use the LO above RF , it means up to 12.8GHz?
any degradation with performances?
(The LTC5548 datasheet limit the max LO frequency to 12GHz)
Roni
KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
LTC5548
Production
The LTC5548 is a high performance, microwave double balanced passive mixer that can be used for frequency upconversion or downconversion. The device is...
Datasheet
LTC5548 on Analog.com
Hi
I would like to use this mixer as Upconverter from 1.3GHz to 11.5GHz
Can I use the LO above RF , it means up to 12.8GHz?
any degradation with performances?
(The LTC5548 datasheet limit the max LO frequency to 12GHz)
Roni
The LTC5548's performance degradation at LO frequencies above12GHz is fairly gradual. Extrapolate the performance from these plots from the datasheet can give you an idea of the amount of degradation: