I was given a nice reliability report with MTTF data on it for nominal operating conditions for the HMC1087F10 8-Watt GaN 10-Lead Flange Chip and was wondering if the same data was available for the HMC998APM5E; I included the Drain Operating Voltage that is currently being used in our application and have worked out the math with the MTTF Formula used in the HMC1087F10 Case, but just wanted to follow-up and make sure there wasn't any manufacturer data that you all had available that I could show as a comparison and to also have to check myself with. Thanks in advance.