Post Go back to editing

Low Frequency RFoutput Power of ADF4356

Category: Datasheet/Specs
Product Number: ADF4356

Hello. 

I use ADF4356 at 100MHz to 300MHz.

The ADF4356 datasheet (Figure 10) shows the variation of RF output with temperature.

Therefore, if you have measurement data showing the relationship between temperature and output power in the range of 100MHz to 300MHz as shown in Figure 10, could you please provide it?

We would be happy if the test conditions were also below.

"For lower frequencies below 2 GHz, it is recommended to use a 100 nH inductor on the RFOUTA+/RFOUTA− pins and a 100 pF ac coupling capacitor."

Best Regards.