MAX2871
Production
The MAX2871 is an ultra-wideband phase-locked loop (PLL) with integrated voltage control oscillators (VCOs) capable of operating in both integer-N and...
Datasheet
MAX2871 on Analog.com
Dears.
We are considering the following:
1. REF_IN None external.
2. Is it possible to output RF OUTA at 250Mhz using only internal VCO?
3. Does REF_IN require external input?
4. I would like to output using only the internal VCO. Is it possible?
5. Can RFOUT be used as a single end?
Thank you