Hi JudeOsems , et.al,
I have follow up questions to the post at Unable to get HMC440 working - Q&A - RF and Microwave - EngineerZone (analog.com).
Specifically concerning what to expect as the output of the loop filter placed after the PFD HMC3716.
I refer to the datasheet of the PFD, that shows what the typical NU/ND signals will look like. Attached below:

I deduce that NU is 2Vp-p with 2V offset sawtooth signal and ND is 5V DC signal. And in my test using the copy of the evaluation board of the HMC3716 that I procured, I could see these signals on my oscilloscope.
But I am not clear on the implementation of loop filter and its output that is meant to drive the VCO. The VCO of choice here is the HMC6380 requiring Vtune up to 23V. And the schematic of the loop filter follows from the ADISimPLL as follows:

I developed the schematic of the loop filter on a custom PCB, and 'built' up the PLL/VCO. Measured outputs on the spectrum analyser is far from what I'd expect from a properly functional/locked PLL. I ascertain that all subparts are working as expected, but not so confident that the loop filter is.
The schematic of the loop filter transferred to the layout is shown:

Measured output on the spectrum analyzer for the developed PLL/VCO looks as follows:

Screenshot of the spectrum analyzer above suggests a constantly swept VCO across a wide range of Vtune.
I therefore isolated the loop filter for testing, and created the test signals from an AWG following NU/ND as will be obtainable from the PFD: NU is sawtooth signal of 1kHz at 2Vp-p and +2V DC offset; and ND is +5VDC. The green trace in the image below is the NU signal:

In following image below, the output of the loop filter is the yellow trace from an input NU signal which is the green trace:

Can you tell if this is the normally expected output of the loop filter? I would have expected DC type of signals that will drive the VCO and not this rail-to-rail type I recorded on my scope. Did I made some errors in implementing the loop filter?
Kindly advise on how to proceed.
regards!