Post Go back to editing

Voltage level for using signal generator to drive crystal input on MAX147x receivers

Thread Summary

The user inquires about using a signal generator as a reference frequency source for the MAX1473. The recommended signal is a 0.5Vp-p sine wave with a 50 ohm output impedance, and a 10nF DC blocking capacitor should be used in series with the XTAL2 input, along with a 10nF shunt capacitor to ground on the XTAL1 input.
AI Generated Content
Category: Hardware
Product Number: MAX1473

I am interested in using a signal generator as the reference frequency source for a MAX1473.

A related FAQ question answers the connections: https://ez.analog.com/rf/w/documents/19315/what-pin-is-the-osc-input-so-that-i-can-drive-it-with-my-max1470-signal-generator-instead-of-using-a-crystal

What would be an appropriate signal amplitude, and driving impedance?

  • I don't think it matters critically.  I would suggest a 0.5Vp-p sine wave from an RF signal generator that has a 50 ohm output impedance.  Note the requirement for the DC blocking capacitor in series with the XTAL2 input, and the shunt capacitor to ground on XTAL1 input.  Both caps should be 10nF (not 1nF).

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.