Post Go back to editing

LT5537 behavior @10.7MHz

Thread Summary

The user is designing a matching network for the LT5537 at 10.7MHz and requested the S11/impedance data. The support engineer provided the input impedance model as a 1.94K resistor in parallel with a 2.59pF capacitor at 11MHz. The user also sought clarification on the 240Ω termination resistor used in the datasheet example at 200MHz, questioning its effectiveness in achieving maximum power transfer.
AI Generated Content
Category: Datasheet/Specs
Product Number: LT5537

Hello support team,

I am trying to design a matching network for the LT5537 from input of 330 ohm at 10.7MHz.

Can you please provide data of its S11/impedance around this frequency?

My intention is to use its differential input in order to get maximum sensitivity.

Thanks!

Parents
  • Hi RoyKV,

    At 11MHz, the LT5537's input impedance can be modeled as a 1.94K resistor in parallel with a 2.59pF capacitor.

  • Thanks,

    I found it difficult to understand the example made in the datasheet on page 9, when a termination resistor of 240Ω was connected in parallel to the AC coupled input of the LT5537 (figure 5).

    I understand the purpose of this resistor (matching the input impedance of the IC to the balun output of 200Ω for maximal power transfer).

    Here are my problems:

    1. Maximum power transfer requires that the load impedance is the complex conjugated of the source impedance. So in our case we need minimal imaginary part of the input impedance.

    2. I calculated that for 200MHz (the example frequency), the input impedance of the termination (neglecting C1 & C2) and the IC input is 2*(240Ω/2 || (1.73KΩ||1/(j*2*π*200MHz*1.45pF)) ~ 214Ω -j44Ω, so it is quite far from the expected 200Ω real part of the impedance. Thus a smaller termination resistor could have made a better job.

    What mistakes did I do?

Reply
  • Thanks,

    I found it difficult to understand the example made in the datasheet on page 9, when a termination resistor of 240Ω was connected in parallel to the AC coupled input of the LT5537 (figure 5).

    I understand the purpose of this resistor (matching the input impedance of the IC to the balun output of 200Ω for maximal power transfer).

    Here are my problems:

    1. Maximum power transfer requires that the load impedance is the complex conjugated of the source impedance. So in our case we need minimal imaginary part of the input impedance.

    2. I calculated that for 200MHz (the example frequency), the input impedance of the termination (neglecting C1 & C2) and the IC input is 2*(240Ω/2 || (1.73KΩ||1/(j*2*π*200MHz*1.45pF)) ~ 214Ω -j44Ω, so it is quite far from the expected 200Ω real part of the impedance. Thus a smaller termination resistor could have made a better job.

    What mistakes did I do?

Children
No Data