Post Go back to editing

Using two ADF5904 to achieve 8-ch Rx for 24 GHz radar. How should the IO control be implemented? (2Tx using ADF4159+ADF5901, 8Rx using two ADF5904))

Thread Summary

The user inquires about controlling two ADF5904 chips for an 8-channel 24 GHz radar receiver using an MCU. The final answer recommends connecting the CLK, DATA, and DOUT pins together, while managing the LE (CS) pins separately for independent control. A diagram illustrating the recommended SPI connection is provided.
AI Generated Content
Category: Datasheet/Specs
Product Number: ADF5904

Hi, 

Using two ADF5904 to achieve 8-ch Rx for  24 GHz radar. How can two ADF5904 be controlled by the MCU? Do the IO interfaces of two chips need to be connected separately to the main control chip for control, or can they be shorted together for control?

Looking forward to your reply. Thanks a lot!

Edit Notes

/
[edited by: Arnold1 at 12:31 PM (GMT -4) on 5 Sep 2024]
Parents
  • Hi Arnold, 

    CLK, DATA and DOUT pins can be connected as they are standard SPI pins. 

    CE pins can also be tied together for ease of control. However, we recommend managing LE pins separately to control both ADF5904 independently. The below diagram shows the recommended SPI connection. LE pin corresponds to the CS pin. 

    Thanks,

    Emrecan

Reply
  • Hi Arnold, 

    CLK, DATA and DOUT pins can be connected as they are standard SPI pins. 

    CE pins can also be tied together for ease of control. However, we recommend managing LE pins separately to control both ADF5904 independently. The below diagram shows the recommended SPI connection. LE pin corresponds to the CS pin. 

    Thanks,

    Emrecan

Children
No Data