Please can any one share the default settings for generating FMCW wave form for 5.7 to 5.8 GHz with EVAL-ADF4158EB1Z.
ADF4158
Recommended for New Designs
The ADF4158 is a 6.1 GHz, fractional-N frequency synthesizer with modulation and waveform generation capability. It contains a 25-bit fixed modulus, allowing...
Datasheet
ADF4158 on Analog.com
Please can any one share the default settings for generating FMCW wave form for 5.7 to 5.8 GHz with EVAL-ADF4158EB1Z.
Hi,
This tutorial might help you to simulate and extract ramp parameters. After deciding the ramp parameters, you can use the eval board GUI to set the register values.
Using ADIsimPLL to Simulate Frequency Ramps on the ADF4158 | Analog Devices
Thanks,
Emrecan
Thank you Very much for your quick response. We have seen this video, when we are checking the signal in spectrum analyzer for more than 20 MHz Bandwidth Specrum is jumping, that is why we want to cross check the basic working settings for the default eval board and verify whether we are in right direction or not.Please, can you share the working design example if you have.
Hi,
ADF4158 GUI provides default register values for 5.8 GHz operation with the EVAL board. After that, you can enter ramp parameters calculated using ADISimPLL.
For example: 
Please be aware that VCO on the evaluation board has a range from 5.725 to 5.875 GHz. The loop filter is designed to have a 20Khz bandwidth.
Thanks,
Emrecan
Thank you very much for your response,