Post Go back to editing

ltc5596 measured data beyond the data sheet

Thread Summary

The user inquired about characterization data for a frequency range of 13.75GHz to 14.5GHz and temperatures of 0 to 60°C, aiming for a 39dB dynamic range with <±1dB error. The final answer stated that no data is available for those specific temperatures, with only data for -55°C, -40°C, 25°C, 85°C, 105°C, and 125°C provided. The user noted that accuracy degrades at the specified temperature extremes and asked for data closer to 12GHz and 15GHz, but no additional data was provided.
AI Generated Content
Category: Datasheet/Specs
Product Number: LTC5596

I'll be using the part between 13.75GHz and 14.5GHz and between 0 and 60degC. Page 8 in the data sheet shows data for 12G and 15G and temperatures of -40, +25, and +85degC. Do you have data closer to the data points I need in frequency and temperature? My requirement is for 39dB dynamic range and <+/-1dB error. I would like <+/-1dB to allow for some margin for other errors.

ChazLuke

  • Hello,

    The datasheet show and data taken at 12GHz shows not much difference in performance between 12GHz and 15GHz. We do get almost 40dB dynamic range with +/- 1dB error between 35 to 85 and performance should closely match between 0 to 60 degrees as well. Dynamic range falls to almost 37 dB when measured at -40 degrees. I checked our folders and cannot find data for the specific 13.75 GHz and 14.5GHz as requested but the performance should closely match that of 12GHz and 15GHz, if any particular discrepancy is observed, please let me know I can further verify performance on one board.

    Thanks,

    Dushyanth.

  • I'm looking for other temperature points 0 and 60degC. The accuracy degrades at the specified temperature extremes. Do you have any data at 12 and 15G closer to these temperature points?

  • Hi,
    We do not have any characterization data at those particular temperatures. We only have data for the plots for the temperatures in TPC sections i.e for temperatures -55C, -40C, 25C,85C, 105C and 125C.