Post Go back to editing

HMC994APM5E Biasing Circuit

Category: Hardware
Product Number: HMC994APM5E

Hi Team,

I have the following queries regarding the HMC994APM5E:

  1. Can you confirm the sequencing to turn on the amplifier? I am considering powering up VGG1 first, then VGG2 (3.5V), and finally VDD (11V). Can VGG and VDD be applied at the same time?

  2. What is the current drawn on VGG1 (-1V) and VGG2 (3.5V)? Is it acceptable to obtain these voltages using a resistor divider circuit?

  3. I am using this amplifier in the Ku-Band. Can I use the suggested Bias-TEE circuit? What will be the loss at a frequency of 18 GHz?

  4. Considering the current drawn is 250 mA at 11V, can I assume the power consumption/heat dissipation to be 2.75W?

Thank You