Post Go back to editing

ADPA1113A

Category: Datasheet/Specs
Product Number: ADPA1113A

What is the acceptable 28V power min/max for ADPA1113AEJZ ?

  • Hi Yuryws,

                         I'm not sure I fully understand what you are looking for. Are you looking for the Min/max rating of the 28 V power supply or, the RF output power.

    Regards,

    jim B

  • Hi Yuryws,

                          

    We have characterized performance at 24V, 28V, and 32V rails.  So you could say your tolerance on the 28V rail is +/-4V.  But there are performance shifts when you change the supply rail.  These are shown in figures 8, 12, 14, 24, 25, 28, 35, 44.  Some of them (like noise figure) don’t change very much but others (like gain) can be more significant. 

    Regards,

    Jim Bedrosian