Hi Team,
I would like to know the maximum RF settling time of HMC8038 switch and video feedthrough parameter of same.
KCC's Quizzes AQQ306 about a fish stick challenge
1. First the quote of the month: " I am so clever that sometimes I don't understand a single word of what I am saying" - Oscar Wilde
2. New quiz AQQ306 about a fish stick challenge:
Here below is a pseudo fish diagram swimming to the right.
Question
View All
October Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Finding Your Circuit Chi — EMC Quiz!
Think you know EMC? Test your knowledge with our 5-question quiz!
Read the blog first, then take the challenge: Finding Your Circuit Chi
Every current flowing creates electromagnetic fields.
Strong EMC design
View All
HMC8038
Recommended for New Designs
The HMC8038 is a high isolation, nonreflective, 0.1 GHz to 6.0 GHz, silicon, single-pole, double-throw (SPDT) switch in a leadless, surface-mount package...
Datasheet
HMC8038 on Analog.com
Hi Team,
I would like to know the maximum RF settling time of HMC8038 switch and video feedthrough parameter of same.
Hello,
RF settling time for the product depends on (i) process variation of part-to-part and (ii)voltage-temperature within a single part. For (i) it is %25 max, for (ii) it is %10 max.
Video feedthrough is 14mV when looking from RFC, 20mV when looking from RF1/2, all other ports are 50-ohm terminated for both cases.
Kind Regards,
Turgut
Hi Ersoz,
From typical(170ns) RF settling time i have to consider %25 max as 212.5ns and %10 max as 197ns.
Is the above value correct?
Yes, that is correct.