Post Go back to editing

Differential to single ended

Category: Hardware
Product Number: ADL5580

I am in the very early stages of a system design which will use both ADC's and DAC's. Both these devices will have a differential analogue interface. For the ADC channel this device could be used as a single ended to differential driver. The question relates to taking the differential output of the DAC and converting to a single ended RF output from the system. Would it be possible to use this device in that operation: obviously I would need to terminate the non-used output from the device and I expect I would need to be careful about trace impedance on the used output. However I am sure that there are 'gotchas' which I am unaware of at this point. (I am not an RF engineer).

The bandwidths are <6 GHz for the ADC channels and <8 GHz for the DAC channel. The reason for exploring this device as an option is that I will be volume limited in the design.

Thread Notes

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.