Post Go back to editing

IQ Modulator and Demodulator for 2.4MHz

Category: Hardware

Dear Experts,

I am beginner and have no background in communication. I need your help to make 2.4MHz IQ Modulator and Demodulator. I couldn't found any IC available for such a low frequency. I am using FPGA to generate an OFDM IQ signal which than needs to modulate with carrier frequency of 2.4MHz. For sake of simplicity I am looking for an IC which have in-build DAC, Up/down convertor (if needed), Local oscillator, mixer.

Parents
  • Hey ,

    I was able to find AD8333 and AD8339. It fits your frequency requirement of 2.4MHz. Including   and  to this inquiry. Should be able to help point you a I/Q modulator with our portfolio, if my recommendation doesn't satisfy your other requirements.

    Regards,

    Dorant

  • Hi Dorant,

    I apolozies for late response and thanks for the support.

    After through the datasheet of AD8333 and AD8339, I understood that these both ICs are only for demodulation. I also need modulation IC.

    As per my requirements AD8333 is good enough, I will not be using the 2nd channel of it. I wonder how these 2 channels and 4 channels could be used.

    Regards,

    YashJ

Reply
  • Hi Dorant,

    I apolozies for late response and thanks for the support.

    After through the datasheet of AD8333 and AD8339, I understood that these both ICs are only for demodulation. I also need modulation IC.

    As per my requirements AD8333 is good enough, I will not be using the 2nd channel of it. I wonder how these 2 channels and 4 channels could be used.

    Regards,

    YashJ

Children
No Data