Hi,all
The following link on the product page is broken:
What are the differences between MAX2870 and MAX2871?
https://maximsupport.microsoftcrmportals.com/en-us/knowledgebase/article/000097816

Best regards,
sss
MAX2870
Production
The MAX2870 is an ultra-wideband phase-locked loop (PLL) with integrated voltage controlled oscillators (VCOs) capable of operating in both integer-N and...
Datasheet
MAX2870 on Analog.com
MAX2871
Production
The MAX2871 is an ultra-wideband phase-locked loop (PLL) with integrated voltage control oscillators (VCOs) capable of operating in both integer-N and...
Datasheet
MAX2871 on Analog.com
Hi,all
The following link on the product page is broken:
What are the differences between MAX2870 and MAX2871?
https://maximsupport.microsoftcrmportals.com/en-us/knowledgebase/article/000097816

Best regards,
sss
There's a web form on analog.com for reporting
website issues like broken links:
https://form.analog.com/Form_Pages/feedback/websiteInfo.aspx
Hi John- san,
Thank you for reply.
I am researching the differences between MAX2870 and MAX2871, and found the following link on the product page:
What are the differences between MAX2870 and MAX2871?
maximsupport.microsoftcrmportals.com/.../000097816
However, the web link is broken.
Please provide the information or materials on the link.
Best regards,
sss
I wish I could help, but I couldn't find the document
on the web. Hopefully someone who works at
ADI will see your question and respond. Good luck,
It would take too long to give an exhaustive list of differences. Basically, the MAX2871 is a more recent device that improves performance and adds new features. To quote the MAX2871 datasheet: "The MAX2871 has an improved feature set and better overall phase noise and is fully pin and software-compatible with the
MAX2870." One can compare the benefits and features section on the front page of the respective datasheets and observe there are new features such as the ability to phase synchronize multiple synthesizers or automatic VCO selection which exist for the MAX2871 but not MAX2870. There are various specs such as max PFD frequency or output power level which are improved in MAX2871 vs MAX2870.