KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
ADF4382A
Recommended for New Designs
The ADF4382A is a high performance, ultralow jitter, fractional-N phased-locked loop (PLL) with an integrated voltage controlled oscillator (VCO) ideally...
Datasheet
ADF4382A on Analog.com
Hi,
I am trying to simulate the ADF4382A in ADIsimPLL. I would like to simulate equally spaced output frequencies from 5-10GHz, but I get an error saying the VCO is out of range, even though the VCO can output this frequency range, by using an output divider.
If I tell the software I would like to simulate just one output frequency at 5GHz, no error occurs.
Is this a bug? Or is there a limitation on the VCO that I don't understand?
Many Thanks,
James
stephenv - Moved from Other Products (EN) to RF & Microwave. Post date updated from Friday, May 3, 2024 7:35 AM UTC to Tuesday, February 3, 2026 9:08 PM UTC to reflect the move.
Hi,
This is happening because ADF4382A variant covers a fundamental range between 11.5GHz and 21GHz, and supports output divider only 2, and 4. This leaves some gaps in the entire frequency range ( between 5.25GHz - 5.75GHz and 10.5GHz - 11.5GHz) which are not supported. Sadly, your settings fall within this range. Although the full ADF4382 version which will be out at a later date (end of summer) will cover the entire frequency range (11GHz - 22GHz).