Post Go back to editing

Is it OK to mix 4 wire SPI(ADF5902, ADF5904) with a 3 wire SPI interface of (ADF 4159).

Category: Hardware
Product Number: ADF 4159

In my custom board, We are planning to interface SPI 4 wire controller with 3 chip selects/latch enable for 3 different devices ADF5902, ADF 5904 and ADF 4159 ICs.

Here, PLL ADF4159 has SPI interface with a 3 wire (CLK, DATA_IN, LE) . However, VCO transmitter ADF5902 and Receiver ADF5904 have 4 wire SPI interface  (CLK, DATA_IN, LE, DATA_OUT) . Now due to lack of pins on output connector, I need to connect using common SPI controller with 3 devices with common Clk, DATA_IN, CE, DATA_OUT with 3 different LE (CS).
Now, Is it ok to mix 4 wire SPI (ADF5902 and ADF5904) with a 3 wire SPI interface of (ADF 4159)? Are there any other constraints I need to take care of ?
Regards,
SP
Parents Reply Children