Post Go back to editing

HMC8411

Category: Datasheet/Specs
Product Number: HMC8411

Hello :)

If I understand correctly, HMC8411 is characterized for bias Vdd = 5V @ 55mA.

In https://www.analog.com/media/en/technical-documentation/data-sheets/hmc8411lp2fe.pdf in Fig.69 it is mentioned also 4V and 3.3V bias option.

If using 4V / 3.3V bias @ 55mA (with Rbias set according to Fig.69) would that change the datasheet characterization of the device?

Or, if using Fig.69 and seting Idq to 55mA it should be the same?

Thank you in advance.

Thread Notes

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.