MAX2831
Production
The MAX2831/MAX2832 direct conversion, zero-IF, RF transceivers are designed specifically for 2.4GHz to 2.5GHz 802.11g/b WLAN applications. The MAX2831...
Datasheet
MAX2831 on Analog.com
Hi!
For a research project I build a 2.4GHz receiving SDR front-end with a MAX2831. Because the chip is only used aas a receiver, the RXTX pin ist permanently pulled to ground. I set up all 16 registers according to the recommendended settings published in the chip manual. The chip is basically working but shows the effect that the DC offset ot the positive IQ outputs drift down from center voltage 1.1V to like 300-400mV and then now giving any output at all. The design is taken from MAX2831 EVM board. All VCC inputs are supplied by 2.85V which arestable. Ther Output is currently simply a 10kOhms resistor between N and P of each I qnd Q. I can change the DC bias my programming it over the SPI. That works to. But no matter if I go up to 1.45V or whatever: After about a minute I apply power, the output DC voltage drifts away. The both N output stay the same, voltage OK, signal OK.I also replaced it by another one, all the same.
Any ideas?
Hello,
Please check RF output tone power levels are stable at I and Q ports. What is the current consumption in Receive mode. What is the input power applied to MAX2831 Rx port.
Thank You
RF products support team.
Hello,
Please check RF output tone power levels are stable at I and Q ports. What is the current consumption in Receive mode. What is the input power applied to MAX2831 Rx port.
Thank You
RF products support team.