Post Go back to editing

Why 470pF + 6.8nH?

Thread Summary

The user asked why a 470pF capacitor and 6.8nH inductor are recommended for the MAX2659 input matching circuit, noting the resonant frequency is 0.09GHz, not 1.5742GHz. The final answer explains that the 470pF capacitor is for DC blocking due to the internal DC bias at the RF IN, and the LC combination is part of the input matching circuit. The actual operating frequency is 1.575GHz, as shown in the datasheet's return loss graph. The configuration is used to amplify a specific frequency range.

View FAQ
AI Generated Content
Category: Datasheet/Specs
Product Number: MAX2659

The MAX2659 requires an off-chip input matching. Only a 6.8nH inductor in series with a DC-blocking capacitor(470pF) is needed to form the input matching circuit.

Why recommend 470pF + 6.8nH??

this LC resonant frequency is 0.09GHz, not 1.5742GHz.

is it to block all bands and then amplify only the corresponding frequency range?

  • Hi

    We are currently looking into this. We'll keep you posted.

    Thanks,

    Mae

  • Hi latte,

    The recommendation according to this FAQ is for the DC blocking due to the DC bias inside the RF IN of MAX2659, and provide/form an input matching circuit.
    Use this table from the datasheet to know the LC combination for the desired Band/frequency of operation.

    The frequency computation might be a combination of the external LC + what's inside the RFN and looking at some of the TPCs in the datasheet, the configuration definitely shows 1.575Ghz frequency of operation. Like the return loss graph:

    And you're right it's used to amplify specific frequency range.

    -Dann

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.