Post Go back to editing

There is only one L1 band port in max2771?

Thread Summary

The user inquired about the MAX2771 supporting L1-band only on one port (MIXIN_HI) and not the other (MIXIN_LO). The final answer clarified that Analog Devices does not have the MAX2771 part, but referred to the single-channel RF front end MAX2769. The user was directed to the Maxim Integrated technical support site for further assistance, but later indicated that support directed them back to EngineerZone. The user also asked if there is a Maxim IC with two receiver ports, each capable of L1-band.
AI Generated Content
Category: Datasheet/Specs
Product Number: MAX2771

Max2771 support L1-band only on one port MIXIN_HI and not the other MIXIN_LO?