Max2771 support L1-band only on one port MIXIN_HI and not the other MIXIN_LO?
MAX2771
Production
The MAX2771 is a next-generation Global Navigation Satellite System (GNSS) receiver covering E5/L5, L2, E6, E1/L1 bands and GPS, GLONASS, Galileo, QZSS...
Datasheet
MAX2771 on Analog.com
MAX2769
Production
The MAX2769 is the industry's first global navigation satellite system (GNSS) receiver covering GPS, GLONASS, and Galileo navigation satellite systems...
Datasheet
MAX2769 on Analog.com
Max2771 support L1-band only on one port MIXIN_HI and not the other MIXIN_LO?
Hey rahulpillai,
Maxim Integrated products are not supported on EngineerZone at this time. Below, I have included the technical support site where you can get assistance for Maxim Integrated products.
EN - https://maximsupport.microsoftcrmportals.com/en-US/tech-support/
Regards,
Dorant
Hello,
I actually did submit a query in that link, and they replied that i have to submit it here in the engineer zone.

Hello,
I actually did submit a query in that link, and they replied that i have to submit it here in the engineer zone.

Apologizes for the confusion. You will receive support from an EZ engineer.
Hello Rahulpillai, please note that MAX2771 IC has 2 ports one for L1 band and another one for L2/L5 band. MIXIN_HI The mixer input is internally matched to 50Ω for L1 band and MIXIN_LO The mixer input is internally matched to 50Ω for L2/L5 band.
Thank You
RF Products Support Team.
is there a maxim IC with 2 receiver port each capable of L1-band?
Thank you
Hello Rahul, please note we don't have part. We have single channel RF front end MAX2769 and link below.
Selection Table for GPS | Parametric Search | Analog Devices
Thank You
RF Products Support Team.