Post Go back to editing

MAX2120 VAS never locks

Thread Summary

The user is experiencing issues with the MAX2120 PLL not locking and VCO autoselection failing, despite using an 8MHz clock and specific register settings to achieve a 1090MHz LO. The final answer directs the user to contact Maxim Integrated's technical support for further assistance, as Maxim products are not supported on EngineerZone.
AI Generated Content
Category: Datasheet/Specs
Product Number: MAX2120

Hey all!

I'm presently trying to use the MAX2120 in a design; in spite of my best efforts, the status registers always report that the PLL is not locked, and that the VCO autoselection has failed.

I'm using an 8MHz clock into the 2120 and the following settings to trying and achieve an LO of 1090MHz:

  • XTAL divide by 2
  • VCO divide-by 2/4: 4
  • R = 1
  • N = 1090

The STATUS registers show the following, I believe indicating that VAS was attempted and failed.

  • POR = 0
  • VASA = 0
  • VASE = 1
  • LD = 0
  • VCOSBR[4:0] = 0b11111
Register Value Description
N_MSB 0x04 N=1090 MSB
N_LSB 0x42 N=1090 LSB
CHARGE_PUMP 0x00 Per datasheet must-set
N/A 0x00 No F-divider on 2120
N/A 0x00
XTAL_REF 0x21 XTAL divide-by 2, R=1
PLL 0xe0 VCO divide-by 4, VAS charge-pump, 1200uA
VCO 0xcc VAS enabled, latch disabled, non-VAS tuning voltage ADC read disabled
LP_FILTER 0x4b Per datasheet default
CONTROL 0x0f Non-standby, baseband gain 15dB
SHUTDOWN 0x00 Nothing shutdown
TEST 0x08 Charge-pump fast lock (per datasheet must-set)
STATUS_1 0x21 !POR, !VASA, VASE, !LD
STATUS_2 0xff VCO band 11111, VAS ADC invalid because VCO register

Given everything I see here, this should result in a lock. The REFOUT pin is displaying the 8MHz clock divided by 2 as expected, ending up at 4MHz, but the PLL is still marked as unlocked and the IQ data looks like just noise. What am I missing? What would get this design to properly lock? The datasheet is sparse on details for this particular IC so it's difficult to tell what VCO could be used in manual mode either. I appreciate anyone's help in getting this going!

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.