Hi
I am using the ADF4150HV with external VCO : DCMO3288-5 (Synergy ) that support 320MHz to 880MHz
the output frequencies 400MHz to 500MHz (Rf Divider =1)
some of the units does not lock in the range 460MHz to 490MHz
See our schematic & plot
We also see that when connecting the spectrum prob to the vco output then it locked
in this case I see very high phase noise (30 higher compared to locked frequencies)
is it due to using frequencies below the 500MHz ?
Roni