ADPA1106
Recommended for New Designs
The ADPA1106 is a gallium nitride (GaN), broadband power amplifier that delivers 46 dBm (40 W) with 56% typical power added efficiency (PAE) across a bandwidth...
Datasheet
ADPA1106 on Analog.com
Can you provide the layout artwork for the 50V drain pulser board that ships with the ADPA1106-EVALZ evaluation board?
PaulCA - Moved from Amplifiers to RF and Microwave. Post date updated from Thursday, February 8, 2024 8:29 PM UTC to Monday, February 12, 2024 12:48 AM UTC to reflect the move.
Hi DavangP,
Attached is the 50 V pulser artwork you requested.
I also would like to share a new 50 V pulser we have recently released, It is called Pulser Plus, it is fully compatible with the ADPA1106. The advantages of the pulser pulse are, on board Vneg generation for the gate bias, a resistor is used to set the desired bias point for the amplifier and is capable of drain pulsing or gate pulsing. The documentation and design files can be found here: Pulser Plus Reference Design for GaN PA Biasing and Sequencing [Analog Devices Wiki]
Regards,
Jim Bedrosian
Thanks Jim....I read the documentation for the Pulser Plus board (specifically the schematic) and its recommended operating conditions are < 300us Pulse width and < 20% duty cycle. If I had to operating a part greater than 300us pulse width and/or 20% duty, do I need to modify the pulser board to support those conditions? Thank you.
Hi DavangP,
In itself the core of the circuit doesn’t really care much about PW, duty-cycle or time-period. As example, the drain can remain fully on all the time. It is actually the case when running Gate Pulsing when you think about it. As for Gate Pulsing, similar comment could be said. The main limitation comes from the power dissipation of the power amp. The maximum pulse-width and period were a requirement defined in the design process.
Now, this being said, there are a few sections in the circuit that must be looked at when it comes to operating at much higher duty-cycles / time periods. I “tagged” them with a double-asterisk in schematic. Resistors R28, R3, R13, R54 and R55. The dissipation for these specific resistors can be important when operating at high duty-cycles. I didn’t want to use physically large resistors for those locations to handle the much higher dissipation that’d come with the wider duty-cycle / longer time periods. So, they are rated for high power surges but would be limited the closer you get to DC. The resistors:
Regards,
Jim B
Hi Jim, In the Pulser Plus Board, You have mentioned the maximum drain current that the board can support as 5A. What is the limiting factor of the load current in this board? Can i connect a PA of 10A load to this Pulser Plus Board?
Also, you are saying that R3 can be used as a load with the operating conditions of 50V, 5A.
The wattage of the R3 in the schematic is 1.5W. But according to the operating conditions, the wattage on the resistor would be 250W which is very high and obiously the resisttor would burn. Thus, how can we operate the board in this condition?
HI Utsech,
In regards to R3. Some added details:

Dissipation decreases at higher ambient temps:

Around 400-500W for 300us (single pulse)

Periodic/Continuous pulses would lower that value.
However, since the point of the resistor is to verify the electrical functionality of the driver, a single pulse should be good enough. If continuous pulses were to be used, a really short duty-cycle (like 1 pulse every minute) could be considered.
• Although R3 is only present for electrical verification as I just mentioned. The real verification can only be done in combination with the use case PA.
Regards,
Jim B
Hi Utsech,
About the current limit. The LTC7000A does provide plenty of information. I’d suggest starting by reading it in more details:
Regards,
Jim B
Thank you for the response Jim. I am testing the pulserplus board. I am supplying 28V.
The gate pulse circuitry is working but the drain pulse is not coming.
When i am providing the drain pulse enable, the drain output is zero with or without connecting the load at the drain output.
I am getting the pulsed signal on the Imon pin from 0V to 1.6V when i just gave the supply.
What may be the reason for this behaviour on the Imon pin. As per the datasheet if Imon pin is above 1.5V, then there must be some overload. But how can the Imon pin detect 1.6V even though i am not connecting any load.
The Resistance value near the Iset pin is 100K. The resistance value near the Imon pin is 20K.
I want to obtain a drain pulse of 28V and 50V.
Please suggest if I have to change any resistance or capacitor values to obtain my desired output.
Hi Utstech,
Here’s what I’d recommend:
Regards,
Jim B
Hi Jim,
I am still observing the tripping. The VDD_PA output pulse is not turning ON completely. The pulse is turning OFF before turning ON fully. This is happening as soon as i turn ON the power supply to the board.
The signal is fluctuating between overload(1.65V which is above 1.5V) and 0V at the Imon pin.
**I am supplying 28V supply and connecting 16ohm load across the VDD_PA and ground.