KCC Quizzes AQQ303 about the radius of a circle
1. Quote of the month: "When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his car" - Will Rogers
2. Quiz AQQ304 about finding the radius of a circle
Good luck, and try to be
View All
August Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Important: Read the blog first . The quiz questions are all based on the content of the blog:
Stay in the loop and win! Read the blog Current Output Driving Industrial Loops , then take our quick five-question quiz for a chance to win a gift card
View All
HMC994APM5E
Production
The HMC994APM5E is a GaAs pHEMT MMIC Distributed Wideband Power Amplifier which operates between DC and 28 GHz. The amplifier provides 15 dB of gain, ...
Datasheet
HMC994APM5E on Analog.com
Hi,
I am planning to use these amplifiers HMC994APM5E & HMC1082LP4E for pulsed application by switching gate voltage between ON & OFF voltages. Please suggest is it okay to proceed like this?
Pathu - Moved from RF and Microwave to Amplifiers. Post date updated from Wednesday, February 7, 2024 5:44 AM UTC to Wednesday, February 7, 2024 5:44 AM UTC to reflect the move.
Dorant - Moved from Amplifiers to RF and Microwave. Post date updated from Wednesday, February 7, 2024 5:44 AM UTC to Wednesday, February 7, 2024 3:54 PM UTC to reflect the move.
Hey Pathu,
Can you provide additional information on this? Is there a specific target time for switching gate voltage in mind. Would you like both devices to operate a nominal operating conditional or do you have specific drain current you are targeting? For HMC994, there are two gate voltages. Are you only interested in pulsing VGG1?
Regards,
Dorant
Hi,
Yes, approximately gate voltage will be switched ON for 500nS on 1mS time period. Drain current will be same as suggested in datasheet. If gate voltage is pulsed, average drain current only get consumed based on the duty cycle. For HMC994, I would like to switch VGG1. Since my application is pulsed I would like to operate these amplifiers in pulsed mode to reduce overall consumption & dissipation
Hey Pathu,
It depends on what you are using to switch the gate voltage on and off. If you are using HMC980 to switch on and off the gate voltage, it would be too slow for your targeted response time. You can see additional information the response time of VGATE (pg.9-10) for HMC980 within this app note AN-1363 (Rev.B) (analog.com).
You would need to find a switch that would not be degraded by negative voltage and would fast enough for your application.
Regards,
Dorant