Post Go back to editing

CN0566 EVK 14GHz

Thread Summary

The user inquires about modifying the CN0566 EVK for 14GHz operation, both in the Tx and Rx paths. The final answer provides a link to MATLAB and Phaser integration and suggests contacting a Mathworks representative for further recommendations. The user also asks about the optimal performance parameters of the Vivaldi and HB100 antennas and encounters issues with the Pluto SDR connectivity in MATLAB and Python. The user seeks detailed specifications and troubleshooting advice for these components.
AI Generated Content
Category: Hardware
Product Number: CN0566

1. CN0566 EVK Board is Developed X Band, Tx Antenna used Vivaldi 10.5GHz shall we make it 14GHz? what are the steps involved while developing the Antenna.
2. CN0566 EVK Rx Band Width 10 to 11GHz, Instead of Centre Frequency 10.5GHz Can we convert it into 14GHz? is there any modification Required?
3. With this EVK what distance will it capture?

 Thanks & Regards

Purna

Parents
  • You could operate it at 14 GHz by changing out the LPF and BPF filters.  There should be other footprint compatible filters from MiniCircuits that will suppress the lower image and allow through the upper image.   So look through this paper, and make the necessary changes:  https://www.analog.com/media/en/reference-design-documentation/reference-designs/cn0566.pdf

    1.  Yes, you can connect up a different transmit antenna for 14 GHz

    2.  The integrated phased array antenna panel only operates between about 10 and 11 GHz.  However, you can solder in SMP connectors and then use SMP cables to connect up to your own 14 GHz phased array antenna.  

    3.  Do you mean comms receive, or radar receive?  Many factors impact the range.  You would have to run an analysis for your signals and setup--perhaps using the Matlab radar toolkit, etc.  

  • Hi Jon.Kraft,

    Thank you for your message.

    CN0566 EVK Ordered & waiting for EVK Dispatch details, Could you please share the updated Schematic, BOM, PCB Design files, Gerber data & etc...

    I appreciate your understanding.

  • Hi Jon.Kraft,

    Thank you for your support,

    Today Matlab to Python shifted the code while Converting the process unable to connect the SDR ( SDR Blue Light Continually Glow, Not blinking ), Even the Pluto SDR folder is not visible in File Explorer, Could you please support what is the root cause, here are the pics for your immediate understanding.

  • Hi Jon.Kraft,


    Thank you for your Support.


    CN0566 EVK Phaser Board Detection is successful up to 100 meters but while testing we are experiencing latency of 3 sec ( Delay ) Detecting the object in GUI.


    Present this EVK is using the Raspberry Pi4 board instead of that can we use Raspberry Pi5, to minimize the latency or Delay? What are the Challenges of upgrading to Raspberry Pi5 Could you please confirm in this regard?


    If not upgrading to Raspberry Pi5 Board, what are other ways to reduce the latency or delay in object detection?

    Thanks & Regards
    Purna

  • We are working on a new device tree to be able to use the Rasp Pi 5, but it will not be ready for a few months.  However, it will be much faster to not use the raspberry pi.  Instead, connect Pluto to your computer, and connect ethernet from computer to the Phaser's Rasp Pi 4.  Then, run Python/Matlab on your computer.

    https://wiki.analog.com/phaser_matlab#getting_started_and_setup

    Even so, there will be some delay.  In a real radar system, the processing is handled by an FPGA or DSP chip.  Phaser is meant only for education and exploration purposes, not for real time radar use.  

  • Hi Jon.Kraft,

    I trust this email finds you in good health. As we transition our projects from Python to MATLAB, we are keen to ensure seamless integration with the CN0566 Phaser. We kindly request your guidance on the following matters:

    1. **MATLAB Compatibility**:
    - Is MATLAB recommended for use with the CN0566 Phaser?
    - Are there any specific limitations or considerations we should be aware of?

    2. **MATLAB PC Specifications**:
    - Processor (CPU): We seek recommendations on clock speed, core count, and threading.
    - Memory (RAM): What are the minimum and recommended capacities?
    - Storage: Could you clarify SSD requirements?
    - Graphics Card (GPU): While optional, any suggestions would be appreciated.
    - Operating System: Which versions are officially supported?
    - MATLAB Version: Is there a specific release you recommend?
    - Essential Toolboxes: We plan to use the RF and Microwave Toolbox, Transceiver Toolbox, and others. Any additional recommendations?

    3. **Questionnaire or Checklist**:
    - Do you have a specific questionnaire or checklist related to MATLAB integration with the CN0566 Phaser?

    We genuinely appreciate your assistance and eagerly await your response. Thank you for your support!

    Thanks & regards,
    Purna
  • Yes, MATLAB works very well with Phaser.  See this link for more details:

    https://github.com/mathworks/Phaser-Control-with-MATLAB/tree/main

    Regarding question #2, please contact your Mathworks representative for their recommendations.

    For question 3, follow the setup instructions here:  https://wiki.analog.com/phaser_matlab

  • Greetings,

    Thank you for your prompt response.

    As we strive to minimize latency in our project, could you advise on the feasibility of interfacing an FPGA with the current CN0566 EVK hardware to attain reduced latency and enhanced FPS? Your expertise on this matter would be highly valued.


  • Hi Jon Kraft.
    Hope you are doing well!

    We are presently working on "X-BAND PHASED ARRAY PLATFORM," and we require the schematic, design file, antenna related file and Gerber file for this project. Your assistance in this matter would be greatly appreciated.

    Thank you!

  • Please see the first reply above, on Feb 8

  • Hi, 

    sorry for the miscommunication, we are referring to the "X-Band Phased Array Platform". we have gone through the link that you mentioned and searched for the same, but we couldn't find any hardware files related to the antenna and other design and Gerber details. Hence, we request you to help us with schematic, design file, antenna related file and Gerber file for the mentioned project. Just to avoid any further confusion  I am attaching the screenshot of the board we are talking about. 

    Thank you!


Reply
  • Hi, 

    sorry for the miscommunication, we are referring to the "X-Band Phased Array Platform". we have gone through the link that you mentioned and searched for the same, but we couldn't find any hardware files related to the antenna and other design and Gerber details. Hence, we request you to help us with schematic, design file, antenna related file and Gerber file for the mentioned project. Just to avoid any further confusion  I am attaching the screenshot of the board we are talking about. 

    Thank you!


Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.