Post Go back to editing

CN0566 EVK 14GHz

Thread Summary

The user inquires about modifying the CN0566 EVK for 14GHz operation, both in the Tx and Rx paths. The final answer provides a link to MATLAB and Phaser integration and suggests contacting a Mathworks representative for further recommendations. The user also asks about the optimal performance parameters of the Vivaldi and HB100 antennas and encounters issues with the Pluto SDR connectivity in MATLAB and Python. The user seeks detailed specifications and troubleshooting advice for these components.
AI Generated Content
Category: Hardware
Product Number: CN0566

1. CN0566 EVK Board is Developed X Band, Tx Antenna used Vivaldi 10.5GHz shall we make it 14GHz? what are the steps involved while developing the Antenna.
2. CN0566 EVK Rx Band Width 10 to 11GHz, Instead of Centre Frequency 10.5GHz Can we convert it into 14GHz? is there any modification Required?
3. With this EVK what distance will it capture?

 Thanks & Regards

Purna

Parents Reply Children
  • Hi, 

    sorry for the miscommunication, we are referring to the "X-Band Phased Array Platform". we have gone through the link that you mentioned and searched for the same, but we couldn't find any hardware files related to the antenna and other design and Gerber details. Hence, we request you to help us with schematic, design file, antenna related file and Gerber file for the mentioned project. Just to avoid any further confusion  I am attaching the screenshot of the board we are talking about. 

    Thank you!


  • You'll need to start a new thread for that product. Actually, each question that you ask should be a new thread.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.