Post Go back to editing

CN0566 EVK 14GHz

Thread Summary

The user inquires about modifying the CN0566 EVK for 14GHz operation, both in the Tx and Rx paths. The final answer provides a link to MATLAB and Phaser integration and suggests contacting a Mathworks representative for further recommendations. The user also asks about the optimal performance parameters of the Vivaldi and HB100 antennas and encounters issues with the Pluto SDR connectivity in MATLAB and Python. The user seeks detailed specifications and troubleshooting advice for these components.
AI Generated Content
Category: Hardware
Product Number: CN0566

1. CN0566 EVK Board is Developed X Band, Tx Antenna used Vivaldi 10.5GHz shall we make it 14GHz? what are the steps involved while developing the Antenna.
2. CN0566 EVK Rx Band Width 10 to 11GHz, Instead of Centre Frequency 10.5GHz Can we convert it into 14GHz? is there any modification Required?
3. With this EVK what distance will it capture?

 Thanks & Regards

Purna

Parents
  • You could operate it at 14 GHz by changing out the LPF and BPF filters.  There should be other footprint compatible filters from MiniCircuits that will suppress the lower image and allow through the upper image.   So look through this paper, and make the necessary changes:  https://www.analog.com/media/en/reference-design-documentation/reference-designs/cn0566.pdf

    1.  Yes, you can connect up a different transmit antenna for 14 GHz

    2.  The integrated phased array antenna panel only operates between about 10 and 11 GHz.  However, you can solder in SMP connectors and then use SMP cables to connect up to your own 14 GHz phased array antenna.  

    3.  Do you mean comms receive, or radar receive?  Many factors impact the range.  You would have to run an analysis for your signals and setup--perhaps using the Matlab radar toolkit, etc.  

  • Hi Jon.Kraft,

    Thank you for your message.

    CN0566 EVK Ordered & waiting for EVK Dispatch details, Could you please share the updated Schematic, BOM, PCB Design files, Gerber data & etc...

    I appreciate your understanding.

  • Hi Jon.Kraft,

    1. Phaser Plot : CN0566 & VIVALDI Antenna when both opposite placed, the Angle detecting up to one meter. After increasing the gap more than a meter plot shown 40 degrees constantly even angle is less. Please comment and suggestion. 
    2. When trying to read the object echo is not detecting in phaser GUI. 
    3. Can we connect two Tx Antennas at a time & functioning ?
    4. After applying 2D FFT in RAW data the 2D array ( 900,num_chirps) is plotted with using of imshow(). Which basis these points are plotting.
    5. How to map these values (900,num_chirps) to range and velocity in the range doppler plot, when the target is detected and track the target by printing the range and velocity in this scenario
    6.  When target is not detected, Plot dividing two parts and receiving unwanted noise, how to eliminate ? as shown in pic.
  • Hi Jon.Kraft,

    The CN0566 evaluation kit (EVK) focuses on signal steering in the receiver (Rx) path rather than the transmitter (Tx), why not in Tx  just curiosity asking the Q?

  • The array is receive only for a couple of reasons:   1.  Many arrays commonly have more receive elements than transmit elements, as receiving an unknown signal generally requires more antenna elements than transmitting a known signal.  2.  This board is primarily an educational learning platform, and receiving a signal is much more visually intresting than beamforming a transmit signal and not being able to see where it has gone.  3.  Finally, it is less power and cost to receive.  It is because the transmit amplifiers use more power and cost more.  

    In reply to your list of questions on 4/18, let me emphasize the second point that I made above.  Phaser is a learning/prototyping platform for phased array radar.  Many of your questions are just things that need to be learned to get a radar running.  I suggest getting a radar textbook and going through chapters, while trying to implement them on Phaser.  I think you will learn a lot, and it will prepare you for building your own real radar system.  

    For the questions that do apply to Phaser:  3.  You can connect two transmitters, but only one is active at a time.  This is a switched transmit system that is used in virtual arrays.    6.  Yes, I think that divergence is due to some small timing mismatch between the sample clock and the multi chirp pulses.  You can calibrate that mismatch out.  Or try increasing the sample rate.  

  • Hi Jon.Kraft 

    Thank you for your support,

    We are trying to configure the Phaser EVK with Matlab, Installed Matlab and the toolboxes and add-ons required for the EVK, and finished the Communication toolbox support package for the Adalm-Pluto SDR configuration steps for EVK. While verifying the connectivity of the Pluto SDR, Unable to solve the below error while running the below command

     “sdr = adi.AD9361.Rx”

    Error using adi.AD9361.Rx

    The specified superclass 'adi.common.Attribute' contains a parse error, cannot be found on MATLAB's search path, or is shadowed by another file with the same name. Could you please follow the pic for the error?

    .

  • This error is because you did not install the "Communications Toolbox Support Package for Analog Devices ADALM-Pluto Radio".   Please make sure you are following all of the steps here:

    https://wiki.analog.com/phaser_matlab

  • Hi Jon.Kraft,

    Thank you for your support,

    Today Matlab to Python shifted the code while Converting the process unable to connect the SDR ( SDR Blue Light Continually Glow, Not blinking ), Even the Pluto SDR folder is not visible in File Explorer, Could you please support what is the root cause, here are the pics for your immediate understanding.

  • Hi Jon.Kraft,


    Thank you for your Support.


    CN0566 EVK Phaser Board Detection is successful up to 100 meters but while testing we are experiencing latency of 3 sec ( Delay ) Detecting the object in GUI.


    Present this EVK is using the Raspberry Pi4 board instead of that can we use Raspberry Pi5, to minimize the latency or Delay? What are the Challenges of upgrading to Raspberry Pi5 Could you please confirm in this regard?


    If not upgrading to Raspberry Pi5 Board, what are other ways to reduce the latency or delay in object detection?

    Thanks & Regards
    Purna

  • We are working on a new device tree to be able to use the Rasp Pi 5, but it will not be ready for a few months.  However, it will be much faster to not use the raspberry pi.  Instead, connect Pluto to your computer, and connect ethernet from computer to the Phaser's Rasp Pi 4.  Then, run Python/Matlab on your computer.

    https://wiki.analog.com/phaser_matlab#getting_started_and_setup

    Even so, there will be some delay.  In a real radar system, the processing is handled by an FPGA or DSP chip.  Phaser is meant only for education and exploration purposes, not for real time radar use.  

  • Hi Jon.Kraft,

    I trust this email finds you in good health. As we transition our projects from Python to MATLAB, we are keen to ensure seamless integration with the CN0566 Phaser. We kindly request your guidance on the following matters:

    1. **MATLAB Compatibility**:
    - Is MATLAB recommended for use with the CN0566 Phaser?
    - Are there any specific limitations or considerations we should be aware of?

    2. **MATLAB PC Specifications**:
    - Processor (CPU): We seek recommendations on clock speed, core count, and threading.
    - Memory (RAM): What are the minimum and recommended capacities?
    - Storage: Could you clarify SSD requirements?
    - Graphics Card (GPU): While optional, any suggestions would be appreciated.
    - Operating System: Which versions are officially supported?
    - MATLAB Version: Is there a specific release you recommend?
    - Essential Toolboxes: We plan to use the RF and Microwave Toolbox, Transceiver Toolbox, and others. Any additional recommendations?

    3. **Questionnaire or Checklist**:
    - Do you have a specific questionnaire or checklist related to MATLAB integration with the CN0566 Phaser?

    We genuinely appreciate your assistance and eagerly await your response. Thank you for your support!

    Thanks & regards,
    Purna
Reply
  • Hi Jon.Kraft,

    I trust this email finds you in good health. As we transition our projects from Python to MATLAB, we are keen to ensure seamless integration with the CN0566 Phaser. We kindly request your guidance on the following matters:

    1. **MATLAB Compatibility**:
    - Is MATLAB recommended for use with the CN0566 Phaser?
    - Are there any specific limitations or considerations we should be aware of?

    2. **MATLAB PC Specifications**:
    - Processor (CPU): We seek recommendations on clock speed, core count, and threading.
    - Memory (RAM): What are the minimum and recommended capacities?
    - Storage: Could you clarify SSD requirements?
    - Graphics Card (GPU): While optional, any suggestions would be appreciated.
    - Operating System: Which versions are officially supported?
    - MATLAB Version: Is there a specific release you recommend?
    - Essential Toolboxes: We plan to use the RF and Microwave Toolbox, Transceiver Toolbox, and others. Any additional recommendations?

    3. **Questionnaire or Checklist**:
    - Do you have a specific questionnaire or checklist related to MATLAB integration with the CN0566 Phaser?

    We genuinely appreciate your assistance and eagerly await your response. Thank you for your support!

    Thanks & regards,
    Purna
Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.