Post Go back to editing

CN0566 EVK 14GHz

Thread Summary

The user inquires about modifying the CN0566 EVK for 14GHz operation, both in the Tx and Rx paths. The final answer provides a link to MATLAB and Phaser integration and suggests contacting a Mathworks representative for further recommendations. The user also asks about the optimal performance parameters of the Vivaldi and HB100 antennas and encounters issues with the Pluto SDR connectivity in MATLAB and Python. The user seeks detailed specifications and troubleshooting advice for these components.
AI Generated Content
Category: Hardware
Product Number: CN0566

1. CN0566 EVK Board is Developed X Band, Tx Antenna used Vivaldi 10.5GHz shall we make it 14GHz? what are the steps involved while developing the Antenna.
2. CN0566 EVK Rx Band Width 10 to 11GHz, Instead of Centre Frequency 10.5GHz Can we convert it into 14GHz? is there any modification Required?
3. With this EVK what distance will it capture?

 Thanks & Regards

Purna

Parents Reply
  • Those that have placed an order for CN0566 on Digikey/Mouser/Newark have had their order completed.  We have some units left in the warehouse, but are these are being quickly depleted.  If you completed your order on Mouser, you should have it very soon.  If not, please contact Mouser.  

Children
  • Hi Jon.Kraft,

    Received EVK-CN0566, Based on Video we are trying to Cable Interfaces. one of the cable not Matching with Videos like PC Interface to Linux Board cable, Cable one end USB A and other side Micro USB. but Linux Board interface connector not matching with Micro USB Connector cable. Please confirm. it looks like a Micro HDMI. Encircled with pics.USB A to Micro USBLinux board connector looks HDMI

  • We have Tested with HB100 & working, How to test with Vivaldi Antenna, Could you please share us any videos.

  • You can find videos and example code on this here:  www.youtube.com/playlist

  • Hi Jon.Kraft

     I'm in need of detailed specifications for the CN0566 EVK's,  Vivaldi & HB100 Antenna optimal performance for my project. Could you provide the following information:

    S11 (Return Loss)  :
    VSWR (Voltage Standing Wave Ratio) :
    Gain :

    Range
    Half Power Beamwidth (HPBW)
    Losses (including insertion loss)
    Sensitivity
    Radiation Pattern
    Polarization
    Impedance


    If there are any other important parameters that I should be aware of, please do share. Your assistance in this matter would be highly appreciated.

  • when running Phaser_findHB100.py getting following error any views on how to debug. 

  • This error is because either your Pluto is not plugged in, or the Pluto firmware is not configured to be dual transmit/receive, or there is an issue with your SD card.  

  • Hi Jon.Kraft,

    1. Phaser Plot : CN0566 & VIVALDI Antenna when both opposite placed, the Angle detecting up to one meter. After increasing the gap more than a meter plot shown 40 degrees constantly even angle is less. Please comment and suggestion. 
    2. When trying to read the object echo is not detecting in phaser GUI. 
    3. Can we connect two Tx Antennas at a time & functioning ?
    4. After applying 2D FFT in RAW data the 2D array ( 900,num_chirps) is plotted with using of imshow(). Which basis these points are plotting.
    5. How to map these values (900,num_chirps) to range and velocity in the range doppler plot, when the target is detected and track the target by printing the range and velocity in this scenario
    6.  When target is not detected, Plot dividing two parts and receiving unwanted noise, how to eliminate ? as shown in pic.
  • Hi Jon.Kraft,

    The CN0566 evaluation kit (EVK) focuses on signal steering in the receiver (Rx) path rather than the transmitter (Tx), why not in Tx  just curiosity asking the Q?

  • The array is receive only for a couple of reasons:   1.  Many arrays commonly have more receive elements than transmit elements, as receiving an unknown signal generally requires more antenna elements than transmitting a known signal.  2.  This board is primarily an educational learning platform, and receiving a signal is much more visually intresting than beamforming a transmit signal and not being able to see where it has gone.  3.  Finally, it is less power and cost to receive.  It is because the transmit amplifiers use more power and cost more.  

    In reply to your list of questions on 4/18, let me emphasize the second point that I made above.  Phaser is a learning/prototyping platform for phased array radar.  Many of your questions are just things that need to be learned to get a radar running.  I suggest getting a radar textbook and going through chapters, while trying to implement them on Phaser.  I think you will learn a lot, and it will prepare you for building your own real radar system.  

    For the questions that do apply to Phaser:  3.  You can connect two transmitters, but only one is active at a time.  This is a switched transmit system that is used in virtual arrays.    6.  Yes, I think that divergence is due to some small timing mismatch between the sample clock and the multi chirp pulses.  You can calibrate that mismatch out.  Or try increasing the sample rate.