Post Go back to editing

CN0566 EVK 14GHz

Thread Summary

The user inquires about modifying the CN0566 EVK for 14GHz operation, both in the Tx and Rx paths. The final answer provides a link to MATLAB and Phaser integration and suggests contacting a Mathworks representative for further recommendations. The user also asks about the optimal performance parameters of the Vivaldi and HB100 antennas and encounters issues with the Pluto SDR connectivity in MATLAB and Python. The user seeks detailed specifications and troubleshooting advice for these components.
AI Generated Content
Category: Hardware
Product Number: CN0566

1. CN0566 EVK Board is Developed X Band, Tx Antenna used Vivaldi 10.5GHz shall we make it 14GHz? what are the steps involved while developing the Antenna.
2. CN0566 EVK Rx Band Width 10 to 11GHz, Instead of Centre Frequency 10.5GHz Can we convert it into 14GHz? is there any modification Required?
3. With this EVK what distance will it capture?

 Thanks & Regards

Purna

Parents Reply
  • CN0566 Delayed from Mouser to Dispatch, Is there any alternate Solution to get the EVK Board ASAP. With Analog Device CN0566 Fabrication files which Manufacturer is Suitable & What are the Challenges. After Fab & Assembly, For Synthesizer Embedded code is available in web? Please Confirm. 

Children