ADRF5160
Recommended for New Designs
The ADRF5160 is a silicon-based, high power, 0.7 GHz to 4.0 GHz, silicon, single-pole, double-throw (SPDT) reflective switch in a leadless, surface-mount...
Datasheet
ADRF5160 on Analog.com
Dear Support Team,
I have questions regarding ADRF5160 RF Switch.
1. What is the second and third harmonics at +35dBm input power level?
2. What is the hot switching limit of this device?
Thanks.
Hi support team, any update on this?
Hi,
1. For the harmonics, we do not have direct measurement data. However, we provided the Third-Order Intercept (IP3) in the datasheet. You can calculate the harmonics based on the IP3. Here is an apps note
PDF. I would also suggest you order an EVB and test on your bench. Let me know if you have any questions about the setup.
2. For the hot switching power, I need to check with the team. What would be your targeted requirement? It will help us analyze the problem.
Regards,
Zheng
Hi Zheng,
Thank you for your response.
2. For hot switching power, I'm targeting at +40dBm.