AD8351
Production
The AD8351 is a low cost differential amplifier useful in RF and
IF applications up to 2.2 GHz. The voltage gain can be set from
unity to 26 dB using a...
Datasheet
AD8351 on Analog.com
Hello ADI,
Our customer used AD8351 in a project. This project required saturation output of the AD8351. However, when AD8351 is saturated, the INH/INL voltage waveform of the same batch of AD8351 is very inconsistent. I checked the manual and there was no introduction to saturation output in the manual. Please refer to the schematic diagram and waveform below. Is this normal? Thanks

.
PaulCA - Moved from Amplifiers to RF and Microwave. Post date updated from Monday, January 29, 2024 7:21 AM UTC to Tuesday, January 30, 2024 12:33 AM UTC to reflect the move.
PaulCA - Moved from Amplifiers to RF and Microwave. Post date updated from Tuesday, January 30, 2024 12:33 AM UTC to Tuesday, January 30, 2024 12:33 AM UTC to reflect the move.
onepiece - Moved from RF and Microwave to Amplifiers. Post date updated from Monday, January 29, 2024 7:21 AM UTC to Tuesday, January 30, 2024 11:11 AM UTC to reflect the move.
onepiece - Moved from RF and Microwave to Amplifiers. Post date updated from Tuesday, January 30, 2024 11:11 AM UTC to Tuesday, January 30, 2024 11:11 AM UTC to reflect the move.
onepiece - Moved from Amplifiers to RF and Microwave. Post date updated from Monday, January 29, 2024 7:21 AM UTC to Tuesday, January 30, 2024 11:15 AM UTC to reflect the move.
onepiece - Moved from Amplifiers to RF and Microwave. Post date updated from Tuesday, January 30, 2024 11:15 AM UTC to Tuesday, January 30, 2024 11:15 AM UTC to reflect the move.
Hello,
Could you please tie VOCM to a defined voltage rather than only decoupling to GND with a cap? Maybe it is already tied to a defined voltage, but not visible on the schematic you shared.
Thanks
Hello,
VOCM is only decoupling to GND with a cap, does the pin have to be tied to a defined voltage ? Thanks
No it doesnt. Wanted to make sure that it stays at Vsupply/2 which is the default case for the part. If Vcm goes to limits, swing headroom might change.
The minor imbalance you observe is probably caused by the load conditions such that impedance seen at INH might be higher than the INL
Hello, my customer is already using different Vcm to test and matching different impedance. Thank you very much.
Hello, my customer is already using different Vcm to test and matching different impedance. Thank you very much.