Hi,
I refer to the available information in the gerber files of the ADPA9002 (and HMC8410) evaluation module where it was stated that:
"ALL .010 AND .014 THRU VIAS TO BE FILLED WITH NON-CONDUCTIVE EPOXY AND OVERPLATED WITH COPPER, BOTH SIDES."
If correctly taking into account the heat generated in the amplifiers, I am wondering how the amplifier and the bottom plate heat sink make excellent thermal contacts if the vias are filled with non-conductive epoxy and not completely filled with copper that has better thermal properties than the epoxy. Can some explanations be given for this fabrication requirements please?
For a custom design and fabrication of the PCB, can you please give more detailed explanation of how to affix the PCB to the heatsink. What glue or solder material is suitable?