Post Go back to editing

HMC963: IP2 and second harmonic detais

Thread Summary

The user is testing the HMC963 amplifier with its evaluation board and observes a significant reduction in the dynamic range from 60 dB at the input to 30 dB at the output, particularly noting a high second harmonic level. The amplifier is operating in the linear region, 10 dB below the OP1dB of 12 dBm. The support engineer is calculating the expected 2nd harmonic curves and will provide IP2/IP3 data. The user confirms the application covers 10 GHz to 26 GHz and asks for details on how the measurements were obtained.
AI Generated Content
Category: Hardware
Product Number: HMC963

Hi team,

i'm testing the amplifier HMC963 with the relative evaluation board.

I attach 2 images:

  1. the first is a CW signal at 10 GHz at the input of the amplifier HMC963. The input power is about -22 dBm
  2. the secon image  is the output of the amplifier at the same frequency.

At the input of the amplifier the signal has a dynamic range of about 60 dB (fundamental power to second harmonic).

At the output of this the signal has a dynamic range of about 30 dB (fundamental power to second harmonic).

Why this?

The amplifier is not working in the saturation region because the the output power is about 0 dBm and the OP1dB is 12 dBm.

Why is the second harmonic level so high?

What are the IP2 values ​​of the amplifier?

Thank you in advance.

Best regards,

Matteo

Parents Reply
  • Hi Dan,

    thanks for the data.

    However, the second harmonic level is high (see the second image of the first message).

     I'll try to summarize:

    • the fundamental power is about -22 dBm at the input of the amplifier;
    • the second harmonic power is about -87 dBm at the input oh the amplifier;
    • the fundamental power is about 0 dBm at the output of the amplifier (correct because the gain is 22 dB);
    • the second harmonic power is about -29 dBm at the output oh the amplifier. 

    Why this? The amplifier works in linear region (10 dB below the OP1dB of 10 dBm), so the input power of - 22 dBm is not too high. Do you agree?

    Thank you in advance.

    Matteo

Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.