I am using ADF4368 to generate 3.6GHz from 120 MHz.
Could you please clarify below queries?
1. Is it okay to combine Power supply groups of 3V3 via single LDO(ADP7158) (1 and 2)?
2. Is it okay to feed single-ended reference clock instead of differential signal. What is the advantage of using Balun?
3. Input signal level of Reference clock is 0.5V - 2.6Vp-p differential. For 100-Ohm system, it is 9dBm and 50-Ohm it is 12dBm . Is the calculation correct? What is the typical voltage level of reference clock?
4. Is there any simulator to check the divider settings (N divider, VCO Divider, VCO frequency select) to validate?
5.If my SYNC is one-shot waveform and it is driven from LTC6952, where the Differential voltage swing is 500mVpk.i.e. Vpk-pk is 1V.Is it okay to be DC-coupled?
6. AC caps are placed after termination for LVDS and before for LVPECL. Reason for this?
7. What is the use of BLEED?
8. When i have multiple ADF4368 and reference clock are not length matched. How should i compensate this phase mismatch at output?