Hello.
I would like to use the AD8364 at IF = 37 MHz.
Figure 3. and Figure 4 in the datasheet are graphs of detection characteristics and temperature variation error at 450MHz, but I need data around the 37MHz.
Can you give me the data around 37MHz?
I would also like data on the detection voltage error versus temperature at lower frequencies for the single-ended input of the AD8364.
Best regards,