Post Go back to editing

HMC783 SimPLL Question

Category: Datasheet/Specs
Product Number: HMC783

I wanted to perform an experiment with an existing design where I increase the internal PFD of the HMC783 chip.  For this configuration I would be using a reference and PFD of 101 MHz.  In looking at the datasheet both of these should be acceptable (reference max = 200 MHz, PFD max in integer mode = 140 MHz).  When I try to create a new model in SimPLL I get an error that states "HMC783 is incompatible with these requirements: PLL Phase Detector frequency too high for HMC783"  I understand this PFD would be too high for a fractional design but I am curious as to why SimPLL is preventing me from moving forward with my integer configuration.  Any insight is appreciated.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.