Post Go back to editing

AD9779A with ADL5385

Thread Summary

The user seeks to interface the AD9779A DAC outputs with the ADL5385 modulator inputs to produce an RF signal. The final answer recommends using 50-ohm bias-setting resistors, 100-ohm AC swing-limiting resistors, and 500-ohm and 250-ohm resistors for LO feedthrough compensation. A low-pass filter, such as a third-order Bessel filter with a 3-dB frequency of 10 MHz, should be placed between the bias-setting and limiting resistors to maintain the dc bias level and filter out noise and images.
AI Generated Content
Category: Hardware

Hello,

As part of our project, we would like to interface the outputs of AD9779a to the inputs of ADL5385 and produce an RF signal that way. We assume we need to implement a filtering/matching/interface circuit between the two. As reference, we used the datasheet of AD9779a, which has one set of component values, on figure 79 page 45. Similarly we checked the schematic of the AD9779a eval board which has a different set of values, and the ADL8385 which has a third set. Please provide us with either a working set of components so that we could best match the AD9779a with ADL5385, or provide a link for the calculation, so that we can hope for the best quality in terms of supression, inbalance etc

  • Hi  ,

    This is to acknowledge your query. We will get back to you as soon as possible. 

    Regards,

    Marco

  • Hi  ,

    There are four parts to consider when designing an interface circuit between the AD9779A and ADL5385:

    1. Bias-Setting Resistors. These resistors establish the bias level from the DAC to the modulator. Thus, their value should be based on the input dc bias required by the ADL5385 (500 mV) and the nominal midscale current of the AD9779A ( ~10 mA). It can be determined from these two that a 50-ohm resistor at each DAC output to ground should be used.
    2. AC Swing-Limiting Resistor. This resistor is added to the interface to decrease the ac voltage swing for a given DAC output current and so depends on the desired voltage swing (see formula and graph obtained from the ADL5375 datasheet below for when a 50-ohm bias-setting resistors are used). To input a 1-Vpp differential swing to the ADL5385 from the AD9779A with a 50-ohm bias-setting resistor at each of its outputs, a 100-ohm limiting resistor should be placed between each side of the differential pair.

    3. LO Feedthrough Compensation. The auxiliary DACs of the AD9779A can be used to compensate for the LO feedthrough when a quadrature modulator such as the ADL5385 is connected to the DAC output. This can be achieved by connecting each auxiliary output through a 500-ohm resistor to ground, and through a 250-ohm resistor to one of the modulator signal inputs.
    4. Low-Pass Filter. When a DAC is used to drive a modulator, a low-pass filter is employed to eliminate noise and images while preserving the dc bias level between the devices. This filter is typically placed between the bias-setting resistors and the limiting resistor to conveniently establish its input and output impedances. Moreover, the filter design depends on the requirements of the application. The ADL5385 and ADL5375 datasheets provide a few examples such as a five-pole Chebyshev filter with a corner frequency of 39 MHz (see ADL5385 datasheet p. 18); a third-order Bessel filter with a 3-dB frequency of 10 MHz (see ADL5375 datasheet p. 25); and a fifth-order Butterworth filter with a 300-MHz corner frequency (see ADL5375 datasheet p. 26). The AD9779A evaluation board (AD9739-DPG2-EBZ) uses the ADL5375 quadrature modulator and has adopted the third filter design.

    For the working set of components, I recommend following the circuit below (Figure 79 in AD9779A datasheet) for the bias-setting, limiting, and LO feedthrough compensation resistors. As for the filter, I suggest choosing from the examples in the datasheet and modifying the design as necessary to fit your requirements.

    Hope this helps.

    Regards,
    Zaeefa

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.