Post Go back to editing

HMC8362 and HMC8364 Vtune port models

Thread Summary

The user inquired about more detailed Vtune interface schematics for the HMC8362 and HMC8364, specifically regarding lot-to-lot capacitance variation and the effect of DC bias on the Vt port. The support engineer confirmed that the capacitance values in the data sheets are nominal and that no simulation results or graphs showing the effect of DC bias are available. The user followed up requesting graphs of Ct vs. Vt, but no additional information was provided.
AI Generated Content
Category: Datasheet/Specs
Product Number: HMC8362LP6GE, HMC8364LP6GE

Re: HMC8362 and HMC8364

Do you have any better information on the Vtune interface schematic than that shown as fig 5 on the data sheets?

The HMC8362 fig 5 shows a total capacitance of 420 pF, and the HMC8364 fig 5 shows a total capacitance of 340 pF, 

How much lot-to-lot variation is expected? Do these values vary with the DC bias on the Vt port?

If so, do you plots or graphs showing the effect of DC bias?

Is these maximum values or simply nominal values?

Thank you.

Doug

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.