Post Go back to editing

HMC8362 and HMC8264 Vtune input models

Thread Summary

The user inquired about more detailed Vtune interface schematics for the HMC8362 and HMC8364, specifically regarding capacitance values, lot-to-lot variation, and the effect of DC bias. The final answer directed the user to a thread discussing Vtune port models, which provides additional information. The capacitance values mentioned are nominal, and the thread includes plots showing the effect of DC bias on these values.
AI Generated Content
Category: Datasheet/Specs
Product Number: HMC8362

Re: HMC8362 and HMC8364

Do you have any better information on the Vtune interface schematic than that shown as fig 5 on the data sheets?

The HMC8362 shows a total capacitance of 420 pF, and the HMC8364 shows a total capacitance of 340 pF.

How much lot-to-lot variation is expected? Do these values vary with the DC bias on the Vt port?

If so, do you plots or graphs showing the effect of DC bias?

Is these maximum values or simply nominal values?

Thank you.

Doug

Edit Notes

moved and updated form
[edited by: GenevaCooper at 2:27 PM (GMT -5) on 20 Nov 2023]

Thread Notes

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.