Post Go back to editing

ADRF5720 power sequence

Category: Hardware
Product Number: ADRF5720

Is there any risk of damage to the ADRF5720 if applying -3.3V before +3.3V?

Parents Reply Children
  • Hi Dan

    Thanks for sharing the waveform. Could you also respond to the following?

    1) What is the decoupling cap value connected to the VDD pin?

    2) Is it possible to measure the voltage drop at the resistor using a differential probe (I am assuming this measurement is from one end of the resistor to the GND)?

    We suggest the correct power-up sequence: VDD is applied before VSS but also wanted to find out the source of the 11mA current value.

    Regards

    Gokhan