Hi all,
We have problems with the output stability of a system based on the AD9542-EVAL. Our system uses AD9542-EVAL to generate a 100 MHz signal that is used as the reference of a IF to Ka frequency converter. AD9542-EVAL output seems to be stable in the spectrum analyzer but, when we observe the Ka output, signal is continuously moving and, weirdly, after several hours, we can see an unlock.
OUTPUT signal (after some seconds)
OUTPUT signal (after 24 hours)
Eval board configuration is shown in the nest picture:
The following zip file contains the cso file of our configuration:
Our IF to Ka converter is used with other references without problems, but, once we connect the AD9542 output, these stability problems start.
We would appreciate any help on this topic. Thank you very much,