Hi
One of our customers wants to do simulations in ADIsimPLL with the ADF4159 and the HMC1162, the ADF4159 is in the tool but I think the HMC1162 is not.
Am I overlooking something? If it is not there, can we make the model available?
Thanks!
Rob
KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
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
HMC1162
Recommended for New Designs
The HMC1162 is a monolithic microwave integrated circuit (MMIC), voltage controlled oscillator (VCO) that integrates the resonator, a negative resistance...
Datasheet
HMC1162 on Analog.com
ADF4159
Recommended for New Designs
The ADF4159 is a 13 GHz, fractional-N frequency synthesizer with modulation and both fast and slow waveform generation capability. The part uses a 25-bit...
Datasheet
ADF4159 on Analog.com
Hi
One of our customers wants to do simulations in ADIsimPLL with the ADF4159 and the HMC1162, the ADF4159 is in the tool but I think the HMC1162 is not.
Am I overlooking something? If it is not there, can we make the model available?
Thanks!
Rob
Hi Rob,
ADISimPLL version 5.60.07 should include the HMC1162 Model.
When you create a new simulation, the VCO selection window appears after setting frequency requirements like below.

In this window, you can select your VCO model. In addition to above method, there is another option to select VCO model.
After the selection loop filter, the ADISimPLL configuration asks for VCO selection (if VCO is not selected on the previous screen). You can select HMC VCO Library and select the VCO from the dropdown menu or you can click the Search VCO Libraries button and select the VCO model from the table.

If you cannot find HMC libraries in your project, You can try to re-install ADISimPLL's latest version or send me an e-mail so I can share the HMC library file with you.
Thanks
Emrecan